Arrow: Driving the future of industry in robotics, industrial IoT, and intelligent automation seminar 2026
Industry-leading power density and innovative architectures of Vicor power modules for robotics, industrial IoT, and intelligent automation
Reducing the scale of any intervention is a common aim in surgery, enabling the patient to recover more quickly. Miniature robotic tools can facilitate a reduction in the scope of the surgery. In addition, linking the position of the tool to a patient’s CT scans improves precision and reduces risk. Reducing the surgeon’s fatigue requires the minimization of the size of hand-held operat-ing tools. This manufacturer had the twin goals of reducing the weight of their hand-held robotic tool and improving its reliability. The key goals were:
Power for the tool came from a 55V medically isolated bus and required conversion to 24V within the tool to drive the motors and control circuitry. To save space and weight a DCM DC-DC converter was selected that provided the 300W required in a footprint of just 8.8 cm2 and a weight of only 24g. The converter featured a low noise switching topology and also provided isolation, helping to reduce EMI from the device.
DCM offered high power density (1kW/in3) and low weight (24g)
Minimal electromagnetic interference (EMI)
DCM’s high level of integration significantly increased reliability
A DCM DC-DC converter converted the 55V input to 24V 300W to drive the motor and control electronics. The high efficiency (91.3%) of the converter reduced waste heat in the tool, improving system reliability. To analyze this power chain go to the Vicor Whiteboard online tool.
電力供給ネットワーク(PDN)
Arrow: Driving the future of industry in robotics, industrial IoT, and intelligent automation seminar 2026
Industry-leading power density and innovative architectures of Vicor power modules for robotics, industrial IoT, and intelligent automation
Digitimes key pathways for unmanned vehicle technology
Learn about high-density power conversion for UAVs
Accelerate your move to a high performance 48V power delivery network
This eBook provides guidance on designing 48V power delivery networks to enhance the performance, efficiency, and reliability of industrial products
Build better UAVs using modular power
Power Delivery Networks (PDN) based on Vicor high performance power modules enable innovative designs for the next generation of UAV development