Skip to main content
EET ASIA Article

Vicor powers universal wireless charging station for UAVs and robots

Smart power systems and enhanced robot intelligence deliver autonomous wireless charging for optimal performance.

WiBotic charging station

The demand for more efficient and flexible recharging solutions is constantly increasing. The real focus is on greater autonomy.

How can a fleet of disparate robots be more efficient with less manual intervention? One way to address the issue is with more efficient and flexible recharging solutions based on innovative power delivery networks using Vicor high-performance, high-density power modules.

WiBotic offers wireless charging and power optimization solutions for the aerial, mobile, marine, and industrial robot market. WiBotic, which designs and manufactures solutions for charging drone and robot batteries, combines both inductive and resonant systems to achieve a more seamless charging experience.  Cloud-based software, APIs and tools ensure that robots reload as quickly as possible when needed or more slowly when route planning is not massive.

“A lot of our innovation for robotics comes on the output of the RF amplifier on the transmitter, and then on the receiver side, the input to the rectifier, that’s where we are able to dynamically tune our systems impedance to make sure that we are maximizing our power transfer by keeping the source and load impedances on both sides of the air-core transformer matched. We’re dynamically tuning and sensing things very quickly in real-time to accommodate movements or disruptions or changes as they happen in the system,” said Ben Waters, WiBotic CEO.

Digram of the WiBotic recharging system

Figure 1:  In the WiBotic recharging system, the transmitting unit generates a high-frequency wireless power signal through the AC source. The signal travels through an SMA coaxial cable to the transmitting antenna coil where it generates both electric and magnetic fields. The coil can be mounted in any orientation.

To achieve efficient and robust wireless charging, WiBotic employs an innovative power delivery network (PDN) that combines GaN technology with Vicor high-performance, high-density power modules.

The Power Delivery Network

WiBotic Power Delivery Network diagram

Figure 2:  The Vicor 48V VI Chip PRM Regulator PRM powers the transmitter on board the WiBotic TR-110 wireless charging station, which wirelessly powers the robot/drone on-board receiver. The PRM accepts 48V from an AC-DC power supply and the output voltage is adaptively controlled and cut off from about 20 – 55V.

The Vicor 48V PRM™ buck-boost regulator is integrated into the RF transmitter onboard the WiBotic TR-110 wireless charging station, which feeds power wirelessly to the robot/UV onboard RF receiver. The PRM accepts 48V from an AC-DC power supply and the output voltage is dynamically controlled and trimmed from approximately 20 – 55V as needed. 

Vicor PRM regulator PRM48AF480T400A00

Resources