Power Corner: Vicor’s Maury Wood on vertical power delivery for AI data centers
Vicor’s 48V Factorized Power ArchitectureTM uses vertical power delivery to cut I2R ...
The best methods for distributing high currents while minimizing resistive and inductive losses.
Strategies to deal with multiple outputs and power levels in nontraditional board spaces.
For over 40 years Vicor has been a trusted U.S. supplier of the most innovative high-performance power solutions for the aerospace and defense market. The Department of Defense (DoD) and many of the defense industry’s top prime contractors and tier 1 suppliers turn to Vicor for their toughest power design challenges. Vicor’s patented power module technology enables defense OEMs to push the limits of their imaginations. So no matter the challenge, Vicor will work hard to deliver a power solution that will exceed your expectations every time.
In this podcast, Robert Gendron speaks with Emerj about how Artificial Intelligence (AI) systems are powered and need to be different than traditional manufacturing equipment. He also discusses how the powering of these systems need to work if businesses want to reduce energy costs and be as efficient as they can when it comes to AI.
Listen to the podcast to learn more about how Vicor is optimizing power for AI
Power Corner: Vicor’s Maury Wood on vertical power delivery for AI data centers
Vicor’s 48V Factorized Power ArchitectureTM uses vertical power delivery to cut I2R ...
DC-DC power modules help to bridge the 48V to 12V transition
Power delivery networks (PDNs) are making a decisive shift from 12V to 48V architectures
Accelerating the transition to 48V power systems
The six things to consider when transitioning to 48 volt power systems
Optimizing DC-DC converter stability: AC and transient analysis in simulations of source impedance effects
Learn how to optimize DC-DC converter stability through AC analysis in the frequency-domain and transient analysis in the time-domain