Current gain and current density essential to power AI today: Patrizio Vinciarelli interview
Patrizio Vinciarelli, CEO of Vicor shares insights on powering AI today and its extraordinary current demands and the need to easily scale
Density of power components has increased several orders of magnitude over the past couple of decades. On one hand this has led to a significant reduction in size and cost of power electronic converters; on the other hand, designing the appropriate cooling solution has become more and more challenging. In many cases, thermal management is the gating item that determines the feasibility of a project, and the thermal management solutions need to be evaluated at a very early stage in the design of a power supply.
To simplify your thermal evaluation Vicor has released several simulation models that enable evaluation of the thermal characteristics of our products. The simulator allows you to do a preliminary evaluation of the functionality of our products in your specific environment and operating conditions. The simulator evaluates whether the operating conditions selected by the user when under the selected cooling option are within specification, or if modification to the selected cooling strategy are needed.Overview of Vicor thermal simulator interface. In this example, the cooling type selected was “Heat Sink”. The Option of a “User Defined Cold Plate” is also available.
With just a few clicks, you can select the Vicor power component you are planning to use, customize your source and load conditions, ambient temperature, and evaluate the feasibility under several possible choices of cooling solutions. These solutions may include various types of Vicor heatsinks, as well as custom defined cold plate solutions. In a few seconds you will be able to determine the ideal cooling approach for your project, and you can proceed with your design knowing that thermal management has been addressed already!
Figure 2: Examples of results returned by the thermal simulation: the top image shows a cooling solution that is adequate for the selected operating conditions; the bottom one shows a cooling solution that is undersized, and provides directions on how to improve the thermal management.
Current gain and current density essential to power AI today: Patrizio Vinciarelli interview
Patrizio Vinciarelli, CEO of Vicor shares insights on powering AI today and its extraordinary current demands and the need to easily scale
ReVolt 正在攻克电影行业最不愿公开的污染问题——二氧化碳排放
ReVolt Fuel 解决了电影行业每年排放 70 万吨二氧化碳的难题,在 Vicor 电源模块的帮助下提供清洁的现场电力
采用 48V 分比式电源架构™为 AI 处理器供电
采用 48V 分比式电源架构™ 克服传统的多相方案限制,显著降低了高需求负载下的 I²R 热损耗
高压至 48V 电源转换的 11 种优化之道
将高压转换至 48V DC 可大幅降低布线成本和重量,显著提升数据中心和工业系统的能源效率